Copy System Template

Perform the following steps to create a copy of the existing template:

  1. Go to Genix Platform > Digital App Center > My Apps > Asset Performance Management > APM Foundation.

  2. Click Template Definition section.

  3. Click System Template tab.

  4. Click icon under Action column of the respective template, which you want to create a copy. A dialog box to confirm the copy action is displayed.

  5. Click Yes to confirm. Template Details tab is displayed.

    You cannot clone the system templates if the status is Pending for Review or Pending for Approval.